General (Library Waveform Carrier)

The General table in the Carrier n node enables you to turn the Imported carrier on and off, and select a saved channel configuration.

The Baseband parameters for the Library Waveform are described in Baseband (Library Waveform).

After a Library Waveform is loaded:

1. General

State

Source Waveform Name

Available Source Sample Rate

Sample Points

State

Double-click or use the drop-down menu to enable or disable the carrier.

Source Waveform Name

Selects the name of the Library Waveform to be loaded into the software.

Available Source Sample Rate

Displays the Source Sampling Rate of the waveform. This parameter is read only and automatically set by the software.

Sample Points

The value is determined from the waveform currently loaded into memory. Waveform Length is directly related to the Oversampling Ratio value selected. The higher the Oversampling Ratio, the larger the waveform. This parameter is read only and automatically set by the software.

Library Waveform Carrier

MSR: Using the Waveform Library Manager

MSR: Generating a Library Waveform